earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: RP-C
Functionalities: Hardware
Product version: 2022
3/11/2022

Zigbee Modules Screw Terminals

The RP controller expansion Zigbee modules have fixed screw terminals for the power input, power output, and light output.

The wiring recommendations are provided separately. For more information, see Wiring .

Zigbee DALI Module Screw Terminals

The Zigbee DALI module is equipped with eight fixed screw terminals.

For more information, see Zigbee DALI Module Screw Terminals .

Zigbee 0-10V Module Screw Terminals

The Zigbee 0-10V module is equipped with eight fixed screw terminals.

For more information, see Zigbee 0-10V Module Screw Terminals .

  • RP Controller Expansion Zigbee Modules
  • RP-C-EXT-ZB-DALI
  • RP-C-EXT-ZB-0-10V
  • Zigbee DALI Module Screw Terminals
  • Zigbee 0-10V Module Screw Terminals
  • Wiring