The 0-10V light modules have four Light outputs, which are designed for control (dimming) of lights with electronic ballasts, LED drivers, and other 0-10V compatible control gear.
The Light outputs support 0-10V lighting control. Power distribution (100 to 277 VAC) to the control gear is not supported but needs to be accomplished with an external power supply.
0-10V light outputs without power distribution
The 2-pole Light output connector has two terminals for 0-10V lighting control:
Analog Output (AO1 to AO4)
Common (COM)
The four analog outputs are independently controlled. The control signal is a DC voltage that varies between 0 V and 10 V.
The 0-10V light module supports both the current sourcing and current sinking standards.
Outputs
|
4, Light 1 to Light 4
|
Output terminals
|
AOn (n: 1 to 4) and COM
|
Analog output voltage
|
0 to 10 VDC
|
Maximum source/sink current
|
10 mA per output
|