Product version: 2022
12/17/2021

Rebinding Widgets References

You can rebind multiple widget references at the same time.

Show More
action_close

You can clone widgets and rebind widgets references.

Cloning widgets

You can clone existing widgets. This is an efficient way to create widgets with similar configuration. The cloned widget can be edited. This makes it possible to make identical widgets that display different variables.

For more information, see Cloning a Dashboard Widget .

Rebind

You can rebind references using Rebind widget references. The reference source must be of the same type and have the same name as the target. You can rebind several widgets at the same time if the target references are of the same name and same type.

For example, you have created widgets for a room called Room A. The widgets refer to an analog value in the folder Room A, called “Temp”. You have an identical room called Room B. The folder Room B also contains an analog value called “Temp”. If you want to use the same configuration of the widgets in Room A on Room B, you clone the widgets for Room A and then you use Rebind widget references to rebind the cloned widgets to the analog value “Temp” in the folder Room B.

For more information, see Rebinding Widgets References .

To rebind widgets references
  1. Right-click the dashboard and click Edit dashboard .

  2. On the Dashboard toolbar , click the Select items button

     
    action_zoom_plus_stroke
    .

  3. Select the widget you want to rebind by selecting the check box in the widget.

  4. Click the Rebind widget reference button

     
    action_zoom_plus_stroke
    .

  5. In the Target field, click the Browse button.

  6. Browse to the folder where the new target is located.

  7. Click Select .

  8. Click OK .

  9. Click Save .

  • How Dashboards Work
  • Clone Widgets and Rebind Widget References
  • Dashboard Widgets
  • Dashboard Toolbar
  • Widget Dialog Box – Layout Tab
  • Adding a Widget to a Dashboard