earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Operator Display
Functionalities: Schedules
Product version: 3.3, 2022
7/22/2021

Multi-State/Enumerated Schedules

A multi-state or enumerated schedule controls objects that have states based on integers or positive whole numbers including zero.

For example, a multi-state weekly schedule is bound to a multi-state value that controls an air handling unit in an office building. It regulates the air circulation Monday through Friday from 08:00 to 17:00, to 2 (occupied) when the schedule is active and 1 (unoccupied) when the schedule is inactive.

 
action_zoom_plus_stroke Multi-state schedule

Multi-state schedule

  • Schedule Types
  • Weekly Events
  • Adding a Weekly Event
  • Editing a Weekly Event