earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Operator Display
Functionalities: Schedules
Product version: 3.3, 2022
7/22/2021

Editing a Weekly Event

You edit a weekly event to change how the state of a value is controlled by the schedule.

Show More
action_close

A weekly event occurs every week for an extended period of time. You can schedule more than one weekly event for each day of the week.

Note:

While weekly events cannot overlap, exception events can. For more information, see Exception Events .

 
action_zoom_plus_stroke Weekly events

Weekly events

If there are any non-routine events, such as holidays, you can use exception events to override the weekly events in the schedule. For more information, see Exception Events .

To edit a weekly event
  1. In Operator Display, on the Device List screen, tap the arrow button

     
    action_zoom_plus_stroke
    to select the device with the schedule for which you want to edit a weekly event.

  2. On the Device screen, tap the Schedules arrow button

     
    action_zoom_plus_stroke
    .

  3. On the Schedules screen, tap the schedule for which you want to edit a weekly event.

  4. On the schedule view screen, tap the weekly event (green) that you want to edit.

    Note:

    If a weekly event was configured as occurring on several days of the week, you must tap on on this event every day to edit or delete it.

  5. On the Edit weekly event screen, select the event value:

    • For analog, multi-state and enumerated schedules: In the Value box, tap + or - to specify the value of the event.

    • For digital schedules: Tap Inactive or Active (Off or On).

  6. Select the time span type:

    • Tap All day to make the event span 24 hours.

    • In the From and To boxes: tap + or - to select the starting and ending times.

  7. In the Days of week box, tap the day of the week this event is active.

  8. Tap OK .

  9. On the schedule view screen, tap Save .

  • Schedule Types
  • Weekly Events
  • Analog Schedules
  • Digital Schedules
  • Multi-State/Enumerated Schedules