earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Operator Display
Functionalities: Schedules
Product version: 3.3, 2022
7/22/2021

Edit Date Range Exception Screen

Use the Edit date range exception screen to add, edit or delete the time span and the value of a date range exception.

 
action_zoom_plus_stroke Edit date range exception screen

Edit date range exception screen

Table: Edit Date Range Exception Screen

Component

Description

Priority

Tap + or - to edit the priority of the event. 1 is the highest priority and 16 is the lowest. For more information, see Exception Event Priorities .

Start date

 
action_zoom_plus_stroke

Tap to select a specific start date or Now to select the current date.

End date

 
action_zoom_plus_stroke

Tap to select a specific end date or Never to indicate the exception does not have an end date.

Start time

Displays the starting time of the event.

End time

Displays the ending time of the event.

Value

Displays the selected value of the event.

 
action_zoom_plus_stroke

Tap to open the Edit exception event screen, where you add a time span and a value. For more information, see Edit Exception Event Screen .

 
action_zoom_plus_stroke

Tap to open the Edit exception event screen, where you edit the time span and the value. For more information, see Edit Exception Event Screen .

  • Schedule Handling
  • Schedules Screen
  • Add Schedule Event Screen
  • Edit Exception Event Screen
  • Exception Events