earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Operator Display
Functionalities: Schedules
Product version: 3.3, 2022
7/22/2021

Adding a Single Date Exception Event

You add a single date exception event to a schedule to make an exception for a specific day in the schedule.

Show More
action_close

An exception event occurs instead of the scheduled weekly events for a single date, date range, calculated date, or calendar.

For example, you create an exception event in March for an intense aerobics class in the gym to open an air vent to 100 % from 06:30 to 17:00 every Wednesday in March. This exception event takes precedence over the regularly scheduled weekly Wednesday events.

When scheduling exception events, you can use three exception types to provide flexibility and control in your schedule.

Single Date Exception Events

A single date exception event can occur on a single day, or you can use the options for the event to occur on more than one day. Options such as Any year and Any day provide flexibility to a single date.

For example, to schedule a single date event to take place every year on October 31, you select the following single date options:

  • Year: Any year

  • Month: October

  • Day of month: 31

  • Day of week: Any day

For more information, see Adding a Single Date Exception Event .

Date Range Exception Events

A date range exception event is an event that lasts over a period of time. In addition to a specific day of month, you can schedule daily exceptions by selecting a Start time and End time to provide the flexibility to a date range.

For example, to schedule an exception event to occur from the first day of July to the last day of August where the priority is 16, but each day from 08:00 to 17:00 the value is 15.50, select:

  • Priority: 16

  • Start date: 2021-07-01

  • End date: 2021-08-31

  • Start time: 08:00

  • End time: 17:00

  • Value: 15.50

For more information, see Adding a Date Range Exception Event .

Calculated Exception Events

A calculated date is an exception event that recurs. Other than a specific month and week, you can select Any month and Any week or Last week , to provide flexibility to a calculated date.

For example, to schedule the Monday of the first week of every month for an exception event, select the following options:

  • Month: Any month

  • Week of month: First week

  • Day of week: Monday

For more information, see Adding a Calculated Date Exception Event .

Calendar Exception Events

A calendar reference allows you to apply an exception event for all dates specified in the calendar. For example, to schedule exception events for all holidays on a calendar, you select the calendar you want to reference and the schedule will follow the holidays created in the calendar.

To add a single date exception event
  1. In Operator Display, on the Device List screen, tap the arrow button

     
    action_zoom_plus_stroke
    to select the device with the schedule to which you want to add a single date exception event.

  2. On the Device screen, tap the Schedules arrow button

     
    action_zoom_plus_stroke
    .

  3. On the Schedules screen, tap the schedule to which you want to add a single date exception event.

  4. On the schedule view screen, tap the add event button

     
    action_zoom_plus_stroke
    .

  5. On the Add schedule event screen, tap Single date exception .

  6. On the Add single date exception screen, in the Priority box, tap + or - to edit the priority of the event.

    Note:

    1 is the highest priority and 16 is the lowest.

  7. In the Year box, tap + or - to select a specific year between 2020 and 2100 , or Any year .

  8. In the Month box, tap + or - to select a specific month between January and December , Odd months , Even months , or Any month .

  9. In the Day of month box, tap + or - to select a specific day between 1 and 31 , Last day , Odd days , Even days , or Any day .

  10. In the Day of week box, tap + or - to select a specific day between Mon and Sun , or Any day .

  11. On the start/end time and value list header, tap the add time span and value button

     
    action_zoom_plus_stroke
    .

  12. On the Edit exception event screen, select the event value:

    • For analog, multi-state and enumerated schedules: In the Value box, tap + or - to specify the value of the event.

    • For digital schedules: Tap Inactive or Active (Off or On).

  13. Select the time span type:

    • Tap All day to make the event span 24 hours.

    • In the From and To boxes: tap + or - to select the starting and ending times.

  14. Tap OK .

    Tip:

    You can add multiple time spans and values to an exception event.

  15. On the Add single date exception screen, tap OK .

  16. On the schedule view screen, tap Save .

  • Schedule Events
  • Exception Events
  • Exception Event Priorities