earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Enterprise Central, Enterprise Server, AS-P
Functionalities: Semantic
Product version: 2022
3/23/2022

Creating a Semantic Navigation Pane

You can add a semantic pane with a specific initial filter.

Show More
action_close

WorkStation has a number of features to help you navigate in the semantic database.

You can access all the features from the Semantic Navigation View in WorkStation.

For more information, see Semantic Navigation View in WorkStation .

You must use the Engineering with Semantic Navigation to be able to navigate in the semantic database.

For more information, see Opening the Engineering with Semantic Navigation Workspace in WorkStation .

Semantic Navigator

Use Semantic Navigator to navigate between related nodes in the semantic model that describes the building and the installed system. Using the semantic navigator, you can enter the building, navigate between floors, rooms and equipment in the semantic model.

The Semantic Navigator contains a filter that filter on Brick types. This speed up navigation in large ontologies.

For more information, see Semantic Navigator in WebStation .

Semantic Information List

Use Semantic Information List to get an overview of all semantic nodes related to the semantic node that is selected in Semantic Navigator. In the list you can filter using Quick filter. You can also the semantic filter icons to filter on point, equipment, system and location.

From the list you can navigate to objects in the EBO database if the object is related to a semantic node. For example, from a semantic node connected to an alarm in the EBO database, you can navigate to that alarm. That means that you can edit an alarm from Semantic Navigation List.

For more information, see Semantic Information List .

Semantic Navigation Panes

You can create Semantic Navigation panes with initial filters. These panes are also supported in WebStation.

For more information, see Creating a Semantic Navigation Pane .

Semantic Search

You can create saved semantic searches. These saved searches are supported in WebStation.

For more information, see Searching for Semantic Objects or Properties .

To create a semantic navigation pane
  1. In WorkStation, in the System Tree pane, select the folder or EcoStruxure BMS server where you want to create the semantic pane.

  2. On the File menu click New object.

  3. In the Create New Object dialog, select Panel .

  4. Enter a name, path and description for the panel.

  5. Click Edit in Wizard .

  6. In the Panel Configuration dialog box, click Add .

  7. In the object list, select Semantic pane .

  8. Enter a name, path and description for the pane.

  9. Click Edit in Wizard .

  10. Click Create .

  11. In the Panel configuration dialog box, click Edit .

  12. In the Display name box, enter a name.

  13. In the Initial filter box, click browse.

  14. In the Semantic Navigator .

  • Semantic Navigation in WorkStation
  • Semantic Navigator in WorkStation