Use the Advanced submenu to peform advanced operations, such as repairing communications or references.
The Actions menu - Advanced submenu
Command |
Description |
Add attachment |
Click to add an alarm attachment to one or several alarms. |
Clear Content Type |
Click to clear a content type applied on a folder or container object. For more information, see Content Types . |
Copy attachments from |
Click to copy alarm attachments from one alarm to one or several other alarms. |
Detect Subnet/Node conflicts |
Click to detect address conflicts in the network. The command finds and presents the neuron IDs of any online devices that share the same subnet/node address. |
Repair references |
Click to repair references when you have moved, renamed, or deleted an object that refers to another object that is offline. For more information, see Copy, Paste, Duplicate, Move, Rename, and Delete . |
Repair server communication |
Click to repair server communication after an EcoStruxure BMS server has been offline. For more information, see Repairing EcoStruxure BMS Server Communication . |
Rebind |
Click to rebind a LonWorks network and clear and recreate all LonWorks bindings. |
Remove all attachments |
Click to remove all alarm attachments from one or several alarms. |
Select Content Type |
Click to select a content type that you want to apply to a folder or container object. For more information, see Content Types . |
Copy properties from… |
Click to choose the object that you want to copy properties from. |
Change Control |
Click to open the Change Control submenu. For more information, see Actions Menu – Change Control Submenu . |