earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Alarms
Product version: 1.9
10/12/2017

Attachment Properties

Use the Attachment properties to edit attachments and configure whether or not the attachments are displayed when the alarm is triggered.

 
action_zoom_plus_stroke Attachment properties

Attachment properties

Table: Attachment Properties

Component

Description

Display on alarm

Select True to automatically open and display the attachment when the alarm is triggered.

Object reference

Enter the path to the item you want to attach to the alarm.

  • Alarm Attachments
  • Adding an Attachment to an Alarm
  • Adding an Attachment to Multiple Alarms
  • Removing an Attachment from an Alarm
  • Removing Attachments from Multiple Alarms