Product version: 3.3, 2022
12/17/2021

Backup Schedules

The EcoStruxure Building Operation database includes a digital schedule that is combined with a default backup rule. Using this schedule and rule, the system automatically backs up all data on an EcoStruxure BMS server every Sunday at 01:00. You can edit the schedule settings for this backup rule, but you cannot delete the schedule and select another.

For more information, see Editing a Backup Schedule .

Important:

If the automatically scheduled backup occurs during a Daylight Savings Time transition, the backup will not occur. To prevent loss of data, change the scheduled backup to a time that does not conflict with your region's Daylight Savings Time transition.

 
action_zoom_plus_stroke Backup on a standalone automation server

Backup on a standalone automation server

You can create a custom backup rule and then modify its schedule. For example, you can create a backup rule that backs up all data on an automation server daily at 02:00.

For more information, see Creating a Backup Rule .

  • Creating a Backup Rule
  • Editing a Backup Schedule
  • Editing a Backup Schedule
  • Backup Rules View