The EcoStruxure Building Operation database includes a digital schedule that is combined with a default backup rule. Using this schedule and rule, the system automatically backs up all data on an EcoStruxure BMS server every Sunday at 01:00. You can edit the schedule settings for this backup rule, but you cannot delete the schedule and select another.
For more information, see Editing a Backup Schedule
.
Important:
If the automatically scheduled backup occurs during a Daylight Savings Time transition, the backup will not occur. To prevent loss of data, change the scheduled backup to a time that does not conflict with your region's Daylight Savings Time transition.
action_zoom_plus_stroke
Backup on a standalone automation server
You can create a custom backup rule and then modify its schedule. For example, you can create a backup rule that backs up all data on an automation server daily at 02:00.
For more information, see Creating a Backup Rule
.