earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Trends
Product version: 1.9
10/12/2017

Creating a Meter Trend Log and Associated Objects

You use the meter trend log to record the value of a meter and handle consumption calculations independent of meter rollover and meter exchange.

Show More
action_close

​The meter trend log is a variable triggered trend log with extra functionality to seamlessly handle consumption calculations independent of meter rollover or meter exchange.

For more information, see Variable Triggered Trend Logs .

You create and configure meter trend logs using WorkStation.

For example, in the figure below, the meter trend log records a meter the 1st of every month. In the middle of February the meter rolls over to 00000. A chart with meter consumption calculation prints the consumption every month.

 
action_zoom_plus_stroke Meter trend log

Meter trend log

When physically replacing an old meter with a new one, you have to configure the meter trend log by adding the settings of the old meter and new meter in the Manage replacement of meter dialog box in WorkStation. These settings are the foundation to handle a meter rollover or calculating consumption though meter replacement. For more information, see Manage Replacement of Meter Dialog Box .

 
action_zoom_plus_stroke Manage replacement of meter dialog box where you enter the values of the new and old meter.

Manage replacement of meter dialog box where you enter the values of the new and old meter.

Note:
  • In order for a meter rollover to be managed correctly in the meter trend log and to ensure logging starts at the correct energy reading value, you enter previous meter and new meter information in the Manage replacement of meter dialog box. For more information, see Managing Replacement of a Meter .

To create a meter trend log and associated objects
  1. In WorkStation, in the System Tree pane, select the folder or SmartStruxure server where you want to create the trend log.

  2. On the File menu, point to New and then click Trend .

  3. In the object type list, select Meter Trend Log .

     
    action_zoom_plus_stroke
  4. In the Name box, type a name for the trend log.

  5. In the Description box, type a description for the trend log.

     
    action_zoom_plus_stroke
  6. Click Next .

  7. In the Logged variable box, enter the variable that you want to log.

     
    action_zoom_plus_stroke
  8. Click the Set unit button

     
    action_zoom_plus_stroke
    .

  9. Select a unit for the trend log values.

     
    action_zoom_plus_stroke
  10. In the Prefix box, select the prefix of the unit.

  11. Click Select .

  12. In the Delta box, enter the minimum value change that triggers a new record.

  13. In the Trigger variable box, enter the variable that triggers the log.

  14. In the Trigger condition box, select when to record the value of the logged variable:

    • Select Change to true to record the value of the logged variable when the trigger variable changes to true.

    • Select Change to false to record the value of the logged variable when the trigger variable changes to false.

    • Select All changes to record the value of the logged variable anytime the trigger variable changes state.

  15. In the Log size box, enter the number of records to be recorded before old records are overwritten.

  16. In the Available trend storage box, check that the available number of records is not exceeded.

  17. In the Clear when enabled box, select True to clear the trend log every time the trend log is enabled.

  18. Click Next .

  19. In the Start time box, enter the time when the meter is installed.

     
    action_zoom_plus_stroke
  20. In the Start value box, enter the value of the meter when it was installed.

  21. In the Min value box, enter the first value of the meter when it rolls over.

  22. In the Max value box, enter the last value of the meter before it rolls over.

     
    action_zoom_plus_stroke
  23. Click Next .

  24. In the Extended Trend Log box, click the Browse button

     
    action_zoom_plus_stroke
    to create an extended trend log and connect it to the trend log.

     
    action_zoom_plus_stroke
  25. Click Create .

     
    action_zoom_plus_stroke
  26. In the Name box, type a name for the extended trend log.

     
    action_zoom_plus_stroke
  27. In the Location box, enter the path where to store the extended trend log.

  28. In the Description box, type a description for the extended trend log.

     
    action_zoom_plus_stroke
  29. Click Next .

  30. In the Monitored trend log box, make sure that the meter log is entered.

     
    action_zoom_plus_stroke
  31. In the Smart log box, select if you want to use smart log:

    • Select True to enable Building Operation software to automatically optimize the transfer rate of records from the monitored trend log to the extended trend log.

    • Select False to manually specify the percentage threshold ​at which the trend log transfers its records to the extended trend log, and then select the percentage​ in the Threshold box.

  32. In the Maximum transfer interval box, select the maximum length of time that can pass between transfers.

  33. In the Transfer trigger variable box, enter a trigger variable to force a transfer of all records from the trend log to the extended trend log, for example, to generate a complete report. For more information, see Extended Trend Logs .

  34. In the Log size box, enter the number of records to be stored before old records are overwritten.

  35. In the Available trend storage box, check that the available number of records is not exceeded.

  36. In the Include in reports box, select True to make the extended trend log available to WebReports, for example, to include the extended trend log in a trend log comparison report.

  37. Click Create .

     
    action_zoom_plus_stroke
  38. In the Trend Log List box, click the browse button

     
    action_zoom_plus_stroke
    to create a trend log list and connect it to the trend log.

  39. Click Create .

     
    action_zoom_plus_stroke
  40. In the Name box, type a name for the trend log list.

     
    action_zoom_plus_stroke
  41. In the Location box, enter the path where to store the trend log list.

  42. In the Description box, type a description for the trend log list.

     
    action_zoom_plus_stroke
  43. Click Next .

  44. In the Display trend log box, confirm that the meter log is automatically entered.

     
    action_zoom_plus_stroke
  45. In the Log space (records) box, enter the maximum number of records to display in the trend log.

     
    action_zoom_plus_stroke
  46. Click Create .

     
    action_zoom_plus_stroke
  47. In the Trend Chart box, click the Browse button

     
    action_zoom_plus_stroke
    to create a new trend chart and connect it to the existing trend log.

  48. Click Create .

     
    action_zoom_plus_stroke
  49. In the Name box, type a name for the trend chart.

     
    action_zoom_plus_stroke
  50. In the Location box, enter the path where to store the trend chart.

  51. In the Description box, type a description for the trend chart.

     
    action_zoom_plus_stroke
  52. Click Next .

  53. In the Time mode box, select the time mode for the trend chart:

    • Select Absolute (start and end time) and then enter a start time in the Start time box and an end time in the End time box to manually specify the x-axis start point and end point. For more information, see Trend Chart Axes .

    • Select Relative (to current time) and then type the time span in the Time span box to automatically adapt the x-axis of the chart to display the current time as the rightmost value. For more information, see Trend Chart Axes .

     
    action_zoom_plus_stroke
  54. In the Auto scale left Y-axis box, select True to automatically adapt the y-axis scale to the trend log series.

     
    action_zoom_plus_stroke
  55. Under Series , click the Add button

     
    action_zoom_plus_stroke
    to display additional trend data in the trend chart.

  56. In the object type list, select Trend Log Series or Real Time Trend Series .

     
    action_zoom_plus_stroke
  57. In the Name box, type a name for the series.

  58. In the Description box, type a description for the series.

     
    action_zoom_plus_stroke
  59. Click Next .

  60. In the Display variable box, enter the variable you want to display in the trend chart.

     
    action_zoom_plus_stroke
  61. In the Weight box, enter the line weight of the series.

  62. In the Show markers box, select True to display a marker for each recorded value.

     
    action_zoom_plus_stroke
  63. Click Create .

     
    action_zoom_plus_stroke
  64. Click Create .

     
    action_zoom_plus_stroke
  65. Click Create .

The meter trend log is now connected to an extended trend log, a trend log list, and a trend chart.

  • Meter Trend Logs
  • Managing Replacement of a Meter
  • Trend Units
  • Log Record Storage
  • Create Object Wizard – Naming the Object Page
  • Create Trend Log Wizard – Configure Meter Trend Log Page
  • Extended Trend Logs
  • Create Trend Log Wizard – Configure Extended Trend Log Page
  • Trend Log Lists
  • Create Trend Log Wizard – Configure Trend Log List Page
  • Trend Charts
  • Create Trend Log Wizard – Configure Trend Chart Page
  • Trend Chart Axes
  • Create Trend Log Wizard – Configure Trend Log Series Page
  • Trend Log Wizard – Initial Meter Settings Page