earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebReports
Functionalities: Reports
Product version: 1.4, 1.5, 1.6, 1.7, 1.8, 1.9
4/14/2015

Creating a Weekly Report Schedule

You create a weekly report schedule when you want the schedule to run on selected days on a weekly basis at a specified time. For example, you can create a schedule to run every Monday and Friday every week at noon, or every Monday and Friday every other week at noon. You can only schedule dashboard reports.

Show More
action_close

To specify how often you want a schedule to run, use the Frequency setting in Schedules. You can select the options shown in the table.

Table: Report Schedule Frequency Options

Option

Description

Example

Once

The report schedule runs one time using the start date and time you specify.

Set the Frequency to Once. Enter today’s date and 1:00 PM for the Start schedule date and time. The report is scheduled to run today at 1:00 PM.

Daily

The report schedule runs every day, every two days, or any number of days that you specify beginning with the Start schedule date and time.

Set the Frequency to Daily, then select Every 2 Days. Enter today’s date and 1:00 PM for the Start schedule date and time. The report is scheduled to run every other day at 1:00 PM beginning with today’s date.

Weekly

The report schedule runs on the days of the week you specify, every x number of weeks beginning with the Start schedule date and time.

Set the Frequency to Weekly, then select Monday and Friday Every 2 Weeks. Enter today’s date and 1:00 PM for the Start schedule date and time. As of today’s date, the report is scheduled to run on Monday and Friday every other week at 1:00 PM.

Monthly

The report schedule runs on the first day of the month, the last day of the month, or on both the first and last day of the month.

Set the Frequency to Monthly, then select First and Last. Enter today’s date and 1:00 PM for the Start schedule date and time. As of today’s date, the report is scheduled to run on the first and last days of the month at 1:00 PM.

To create a weekly report schedule
  1. In WebReports, on the menu bar, click Schedules .

  2. In the Select existing schedule box, select New schedule .

     
    action_zoom_plus_stroke
  3. In the Report schedule name box, type a name for the schedule.

  4. In the Schedule description box, type a description for the schedule.

  5. In the Select a dashboard report box, select the dashboard report that you want to schedule.

  6. In the Frequency box, select Weekly .

  7. In the Start schedule box, enter the date and time that you want to activate the schedule.

  8. In the Days boxes, select the days that you want the schedule to run on a weekly basis.

  9. In the Every x Week(s) box, type how often you want the schedule to run. For example, type 1 if you want the schedule to run every week, type 2 if you want the schedule to run every other week.

  10. In the Report output format box, select the file format to be used when the report is generated.

  11. In the Report output destination box, type the directory path for the report output.

    Important:

    The report is written to the specified destination using the System account of the Reports Server. If you plan to save scheduled reports to a network drive, ensure that the System account has write access to the network drive.

  12. Select the Overwrite prior report output box, to keep only the most current copy of the report.

  13. Clear the Disable schedule box.

  14. Click Save .

  • Schedules for Dashboard Reports
  • Report Schedule Frequency
  • Creating a One Time Only Report Schedule
  • Creating a Daily Report Schedule
  • Creating a Monthly Report Schedule
  • Editing a Report Schedule
  • Disabling a Report Schedule
  • Deleting a Report Schedule
  • Schedule Reports Page