earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WorkStation
Functionalities: Trends
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022
10/25/2018

Displaying or Hiding Events in a Trend Log List

You hide or display events in a trend log list to make the reading easier. Events that have a value or comment cannot be hidden and are always displayed. For example, as a Record was added, or as a Record was commented.

Show More
action_close

A trend log list displays all values in the trend log in a list.

You can create a trend log list directly from a trend log and refresh the values.

You can manually add records to a trend log list for any type of trend log.

Trend Log List Display

A trend log list can be displayed in a number of ways.

For more information, see Trend Log List Display .

Export of Trend Log Lists and Records

Trend log lists and records can be exported in two different formats:

  • CSV

  • XML

For more information, see Export of Trend Log Lists and Records .

 
action_zoom_plus_stroke Trend log list

Trend log list

To display or hide events in a trend log list
  1. In WorkStation, in the System Tree pane, select the trend log list you want to display.

  2. On the Trend Log List toolbar, click the Events button

     
    action_zoom_plus_stroke
    .

Events are now displayed in the trend log list. Repeat the procedure to hide the events.

  • How Trend Logs Work
  • Trend Log Lists in WorkStation
  • Refreshing a Trend Log List
  • Trend Log List Toolbar
  • Trend Log List Event Icons