Functionalities: User Management
Product version: 3.2, 3.3, 2022
10/15/2020

Log On Methods

The EcoStruxure Building Operation software provides two methods to log on to the system: as a Windows user or as an EcoStruxure Building Operation user.

Log On as a Windows User

If you are logged on with a Windows user account that is mapped to the Windows Active Directory user account group that you belong to, you can select an EcoStruxure BMS server and log on in a single sign-on. For more information, see Logging on to WorkStation using your Windows user account .

You can also log on using another Windows account that is mapped. For more information, see Logging on to WorkStation as another Windows User .

Log On as an EcoStruxure Building Operation User

When logging on as an EcoStruxure Building Operation user, you authenticate yourself with an EcoStruxure Building Operation account user name and password. For more information, see Logging on to WorkStation as an EcoStruxure Building Operation User .

You also select which EcoStruxure Building Operation domain and EcoStruxure BMS server that you want to access. For more information, see User Accounts and User Account Groups .

With an EcoStruxure Building Operation user account, you can also connect directly to the local domain of an EcoStruxure BMS server. For more information, see Administration Accounts in EcoStruxure BMS Server Local Domain .

Password Administration

As a WorkStation administrator, you can change users’ passwords, force users to change their passwords at next logon, or enable and disable the possibility for users to change their passwords.

For more information, see Password Administration .

  • Logging on to WorkStation using your Windows user account
  • Logging on to WorkStation as another Windows User
  • Logging on to WorkStation as an EcoStruxure Building Operation User
  • Windows Active Directory User Groups
  • User Accounts and User Account Groups
  • Administration Accounts in EcoStruxure BMS Server Local Domain
  • Password Administration
  • User Account Management Overview
  • Resolving Enterprise Server or Enterprise Central Port Conflicts