Schneider Electric recommends that you install the license server framework before other Building Operation software or SmartStruxure server devices. The license server installation is included in the License Administrator license package. During the installation of WorkStation or Enterprise Server, the installation software asks for the address to the license server.
License files used to activate time-limited local licenses can be distributed under certain circumstances.
For more information, see Local Licenses .
Plan the license management carefully and purchase network licenses early to avoid unexpected operational stops caused by expired local licenses.
This work flow describes a Building Operation system where license server and Enterprise Server are located on the same computer.
To install Building Operation smoothly use the following installation order:
Installation and configuration order
Number, client/server |
Description |
1. License Server |
|
2. Enterprise Server |
|
3. Workstation |
|
4. other applications |
|
If network licenses are not purchased or are missing, local licenses can be activated from license files. Replace local licenses with purchased licenses before the local licenses expire.