The Enterprise Server time and date settings are configured through the operating system settings on which the Enterprise Server is installed. The time zone offset, configured through the Enterprise Server, is added by Building Operation to the UTC time. The Enterprise Server time zone settings are therefore independent of the operating system time zone settings.
The Enterprise Server uses the operating system clock on which the server is installed. Time zone offset and DST are then added by Building Operation to the UTC time.
To adjust your operating system clock, refer to your manufacturer’s manual for the operating system. The Enterprise Server time zone is configured on the Enterprise Server through WorkStation
The Date and Time synchronization for Automation Server do not affect the Enterprise Server clock. For more information, see Synchronize Network Time Settings .