earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Trends
Product version: 1.9
10/12/2017

Trend Chart Properties

Use the Trend Chart Properties dialog box to configure the general properties of the trend chart.

 
action_zoom_plus_stroke Trend Chart properties

Trend Chart properties

Table: Trend Chart Properties Table

Property

Description

Time mode

​Select the time mode of the x-axis.

Start time

Enter the absolute start time when Time mode is set to Absolute . This time is the leftmost point of the x-axis.

Time span

Type the relative time span of the x-axis.

Time zone

Select the time zone of the trend log list. The mode is the perspective in which the trend log is displayed.

Show nearest information for all series

Select True to show information on every series along a diagonal line.

Show grid lines for X-axis

Select True to show grid lines for the x-axis.

Chart title

Enter the property reference or relative property reference to the folder or other container whose name you want to include in the trend chart title.

Auto scale left y-axis

Select True to activate auto scale and have the left y-axis adapt itself to the displayed series.

Left y-axis minimum

Enter the minimum value of the left y-axis.

Left y-axis maximum

Enter the maximum value of the left y-axis.

Auto scale right y-axis

Select True to activate auto scale and have the right y-axis adapt itself to the displayed series.

Right y-axis minimum

Enter the minimum value of the right y-axis.

Right y-axis maximum

Enter the maximum value of the right y-axis.

Show grid lines for left Y-axis

Select True to show gridlines for the left y-axis originating from the y-axis scale.

Show grid lines for right Y-axis

Select True to show gridlines for the right y-axis originating from the y-axis scale.

 
action_zoom_plus_stroke

Add

Click to add a series to the trend chart. For more information, see Create Object Wizard – Naming the Object Page .

 
action_zoom_plus_stroke

Edit

Click to edit a selected series. For more information, see Trend Chart Series Properties .

 
action_zoom_plus_stroke

Remove

​Click to remove a selected series.

  • Trend Charts
  • Trend Chart Y-Axis has Scale Problems
  • General Information Properties – Basic Tab
  • References Tab
  • Trend Chart Properties