Use the Basic tab to configure the Variable triggered trend log.
Variable triggered trend log properties - Basic tab
Component |
Description |
Status |
Displays the status of the trend log. |
Enabled |
Displays True if the trend log is enabled. |
Logged variable |
Enter the variable you want to log. |
Delta |
Select the minimum value change that triggers a new record. |
Trigger variable |
Enter the variable that triggers the trend log to start recording. |
Trigger condition |
Select when you want the variable recorded: when the trigger variable changes to True, changes to False, or at all changes. For more information, see Variable Triggered Trend Logs . |
Log size |
Select the number of records to store before old records are overwritten, including internal records generated by the trend log. For more information, see Log Record Storage . |
Clear when enabled |
Select True to clear the trend log when it is enabled. |