earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WorkStation, WebReports
Functionalities: Reports
Product version: 1.2, 1.3, 1.4, 1.5, 1.6, 1.7, 1.8, 1.9
5/21/2015

Viewing a Default Report in WorkStation

You view a default report when you want to see a report about a Building Operation alarm, generic object, SmartStruxure server, trend log, or user account.

Show More
action_close

A default report provides information about alarms, generic objects, SmartStruxure servers, trend logs, and user accounts. The report is formatted according to a template that is assigned to a Building Operation object type. You view default reports in WorkStation using the View...Report submenu. You cannot view default reports using a Web browser.

When you install WebReports, default report templates are assigned to the following Building Operation object types:

  • Alarm

  • Generic Object

  • SmartStruxure server

  • Trend log

  • User Account

To view a default report for a single object, you select the object and then the View...Report submenu in WorkStation. While in List View, you can select more than one object of the same type and generate a report for both objects. For example, suppose you want to see a default report about an Out of Range Alarm and an Inside Range Alarm. You can select both alarms in List View and then run View....Report. The default report generates output about both alarms in one report.

You assign templates to object types for the default reports using the Assign Default Reports menu option at the WebReports Web site.

To view a default report in WorkStation
  1. In WorkStation, select an object, such as an alarm, SmartStruxure server, trend log, or user account.

  2. On the Actions menu, point to View and then click Report .

     
    action_zoom_plus_stroke
  • Default Reports
  • Actions Menu – View Submenu
  • Assigning a Default Report Template
  • Assign Default Reports Page
  • Viewing a Default Report with Multiple Objects