earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: WebReports
Functionalities: Reports
Product version: 1.6, 1.7, 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
12/16/2021

WebReports Configuration

You configure WebReports to create and view reports in the Work area of WorkStation. You need to create and configure user accounts to have access to WorkStation and to run, view, and customize reports in WorkStation and the WebReports Web Site.

Report Manager Configuration

Before you can generate, view, and create reports in WorkStation, you need to configure certain parameters using Report Manager in WorkStation.

For more information, see Report Manager Configuration .

WebReports User Accounts

You create and configure user accounts for the WebReports Web site in WorkStation. User accounts that have access to WorkStation also have access to the WebReports Web site. User accounts that do not have access to WorkStation, or whose accounts have expired, do not have access to the WebReports Web site. By default, all user accounts that have access to WorkStation, can run, view, and customize reports in WorkStation and at the WebReports Web site. When you access WebReports through the WebReports Web site, you can perform administrative tasks in addition to viewing and creating reports. To perform the administrative tasks, your user account needs to belong to the Reports Administrators user group.

For more information, see WebReports User Accounts .

WebReports Administrator - Enterprise Server Configuration

WebReports Administrator is a configuration tool to configure the SystemReportsService user account password in the Reports Server. The SystemReportsServer user account password should be same in Enterprise Server and Reports Server to have proper communication between the two servers.

For more information, see WebReports Administrator - Enterprise Server Configuration .

  • WebReports Overview
  • Report Manager Configuration
  • WebReports User Accounts
  • WebReports Administrator - Enterprise Server Configuration