Use the Calculated Exception View in the Schedule Event Properties dialog box to schedule recurring exceptions.
Schedule event properties dialog box – Calculated exception view
Component |
Description |
All Day |
Select to create an all day event. |
Value |
Enter a value for the exception event. |
At |
Enter the start time for the exception event. |
Until |
Enter the end time for the exception event. |
Exception name |
Type a name for the event. |
Exception priority |
Select a priority number between 1 (highest priority) and 16 (lowest priority). |
Event type |
Select Calculated . |
Month |
Enter the month when the calculated exception event occurs. |
Day of month |
Enter the day of month when the calculated exception event occurs. |
Day of week |
Enter the day of week when the calculated exception event occurs. |