Use the Calendar Reference View in the Schedule Event Properties dialog box to reference a calendar to apply to your schedule.
Schedule event properties dialog box – Calendar reference view
Component |
Description |
All Day |
Select to create an all day event. |
Value |
Enter a value for the exception event. |
At |
Enter the start time for the exception event. |
Until |
Enter the end time for the exception event. |
Exception name |
Type a name for the event. |
Exception priority |
Select a priority number between 1 (highest priority) and 16 (lowest priority). |
Event type |
Select Calendar . |
Value |
Enter the calendar you want to use. |
Open calendar |
Click to open the selected calendar for viewing or editing. |