earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Alarms
Product version: 1.9
12/14/2016

Creating a Cause Note

You create a cause note to connect it to an alarm, and to simplify the reporting of the causes that triggered the alarm.

Show More
action_close

A cause note specifies the problem that caused the alarm. Cause notes are grouped by category, with possible alarm causes listed in each group. When an alarm is triggered, you can easily report the causes that triggered the alarm by selecting the predefined choices.

 
action_zoom_plus_stroke Cause Notes dialog box

Cause Notes dialog box

Reporting the cause of the alarm is either voluntary or mandatory. You can configure the alarm so the user is required to report the causes when certain events occur, such as when an alarm is disabled.

​Cause notes can be of great use the next time the same alarm is triggered or when extracting alarm statistics.

To create a cause note
  1. In WorkStation, on the Tools menu, click Control Panel .

  2. On the Control Panel toolbar, select the SmartStruxure server.

     
    action_zoom_plus_stroke
  3. Click Cause notes .

  4. In the Cause notes view, click the Add cause note button

     
    action_zoom_plus_stroke
    .

     
    action_zoom_plus_stroke
  5. In the Add Cause Note dialog box, in the Name box, type the name of the new cause note.

     
    action_zoom_plus_stroke
  6. In the Group name box, type a name to create a new group or select an existing group that the new cause note belongs to.

  7. In the Description box, type a description for the cause note.

  8. Click OK .

  9. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Editing a Cause Note
  • Alarm Control Panel – Cause Notes View
  • Cause Notes