earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: WebReports
Functionalities: Reports
Product version: 1.7, 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
12/16/2021

Energy Monitoring Consumption Report

The Energy Monitoring Consumption report compares the energy consumption of one or more power meters with a target value. You can select a period or date range, as well as specific meters and buildings. The report compares the same or multiple meters over the same or different periods.

The following table shows the input parameters for the report.

Table: Energy Monitoring Consumption Input Parameters

Input Parameters

Description

Utility type

Specifies the type of utility (gas, electricity, or meter).

Power meter

Specifies the meter or site included in the report.

Start report date/time

Specifies the start date and time for reporting on the energy consumption.

End report date/time

Specifies the end date and time for reporting on the energy consumption.

Date filter

Specifies the date range of an operation, such as an alarm trigger, the running of a report schedule, or a read by the Reporting Agent.

For example, if you select Last 7 days for an alarm report, the report displays information about all alarms that were triggered during the last 7 days. If you select Last 7 days for the Report schedule report, the report displays information about all Report schedules that were run during the last 7 days. If you select Last 7 days for the Reporting Agent report, the report displays information about all Reporting Agent reads that occurred during the last 7 days.

Select Fixed date if you entered a Start report date/time and an End report date/time .

Group interval

Specifies the time interval, such as daily, weekly, for organizing and displaying the energy consumption data.

Consumption target

Specifies a comparative value. When the report runs, the actual energy consumption units are compared to the target value.

  • Factory Supplied Reports
  • Energy Monitoring Reports
  • Creating the Energy Folder
  • Creating a Site
  • Configuring a Site
  • Creating a Meter
  • Configuring a Meter
  • Associating an Extended Trend Log with an Energy Meter
  • Energy Object Tagging
  • Attaching a New Tag to an Energy Object
  • Attaching an Existing Tag to an Energy Object
  • Deleting an Energy Object Tag
  • Site Properties – Basic Tab
  • Energy Folder Properties – Basic Tab
  • Electricity Meter Properties – Basic Tab
  • Gas Meter Properties – Basic Tab
  • Meter Properties – Basic Tab