Use the Objects and trends dialog box to view trend objects that are related to one or several selected objects or object properties.
Objects and trends dialog box when you have selected only one object or property.
Objects and trends dialog box when you have selected several objects, properties, or graphic components or groups containing bound properties.
Property |
Description |
[Quick filter] |
Enter a word or a character to filter on. For more information, see Quick Filter . |
Objects |
Lists the available objects, for example, the bound properties of a graphic component. |
Trends |
Lists the trends related to the selected object or property |
Path |
Displays the path of the object, property, or trend selected in the list. |