earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Commission, IP-IO , MP-C, MP-V, RP-C
Functionalities: Engineering, BACnet/IP devices
Product version: 3.3, 2022
7/19/2021

Performing a Factory Reset on the Bluetooth Adapter

You perform a factory reset on the Bluetooth Adapter to erase the current PIN.

Show More
action_close

The SpaceLogic Bluetooth Adapter allows you to establish a Bluetooth connection to MP and RP controllers. You plug the SpaceLogic Bluetooth Adapter into the corresponding SpaceLogic Sensor to connect to the controller. The adapter communicates with the BACnet/IP controller over the sensor bus using an RS-485 cable. For more information, see Connecting SpaceLogic Sensor Devices to an MP Controller .

Notice

SPACELOGIC SENSOR OR OTHER EQUIPMENT DAMAGE

  • Plug in the adapter with the button to the front.

  • Do not plug into any device other than a SpaceLogic Sensor.

Failure to follow these instructions can result in equipment damage.

For more information, see Commission Mobile Application Overview .

 
action_zoom_plus_stroke SpaceLogic Bluetooth Adapter connectivity
Figure: SpaceLogic Bluetooth Adapter connectivity

RP Controller Onboard BLE

You can use Bluetooth Low Energy (BLE) to connect both RP and MP controllers. BLE provides you with the ability to commission BACnet/IP controllers before there is an IP network infrastructure configured and also improves on-site commissioning times and productivity. With the RP controller, you connect using its onboard BLE or the BLE adapter and the SpaceLogic Sensor. In the MP controller, you connect using the Commission mobile application BLE adapter through the controller's sensor bus.

For more information, see RP Controller Onboard BLE .

Connecting to a Controller with the SpaceLogic Bluetooth Adapter

The SpaceLogic Bluetooth Adapter allows you to establish a Bluetooth connection to MP and RP controllers. To connect to a device through the SpaceLogic Bluetooth Adapter, a SpaceLogic Sensor must be wired to the controller.

For more information, see Connecting to a Controller with the SpaceLogic Bluetooth Adapter .

Changing the PIN of the SpaceLogic Bluetooth Adapter

You change the PIN of the SpaceLogic Bluetooth Adapter for best security practices. The SpaceLogic Bluetooth Adapter PIN is engineered to a default code of 333666 and should be changed to a secure code before you perform device commissioning.

For more information, see Changing the PIN of the SpaceLogic Bluetooth Adapter .

Updating the SpaceLogic Bluetooth Adapter Firmware

You update the SpaceLogic Bluetooth Adapter firmware to improve adapter performance.

For more information, see Updating the SpaceLogic Bluetooth Adapter Firmware .

Performing a Factory Reset of the SpaceLogic Bluetooth Adapter

You perform a factory reset on the SpaceLogic Bluetooth Adapter to erase the current PIN.

For more information, see Performing a Factory Reset on the Bluetooth Adapter .

SpaceLogic Bluetooth Adapter LED Functionality

The SpaceLogic Bluetooth Adapter LED light displays different sequences to indicate the various functionality.

For more information, see Bluetooth LED Functionality .

To perform a factory reset on the Bluetooth Adapter
  1. Connect the Bluetooth Adapter to the SpaceLogic Sensor.

  2. Press and hold the LED push button for 25 seconds.

The Bluetooth Adapter has been reset to its factory setting. The PIN has been reset to 333666. Your mobile device or Windows 10 laptop will need to reconnect to the Bluetooth Adapter and you will need to enter the factory PIN before connecting to the adapter.

  • SpaceLogic Bluetooth Adapter