Use the Initial Meter Settings page to set the initial values for the meter.
Initial Meter Settings page
Property |
Description |
Set initial meter |
Select True to enable the meter function. |
Start time |
Enter the time when the new meter was installed. |
Start value |
Enter the value of the new meter when it was installed. |
Min value |
Enter the first value of the new meter after roll-over. |
Max value |
Enter the last value of the new meter before roll-over. |