earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Functionalities: Trends
Product version: 3.2, 3.3, 2022
10/15/2020

Meter Function

​The meter function adds meter properties to any trend log type to seamlessly handle consumption calculations independent of meter rollover or meter exchange.

You create and configure the meter function in trend logs using WorkStation.

For example, in the figure below, the meter function in the trend log records a meter the 1st of every month. In the middle of February, the meter rolls over to 00000. A chart with meter consumption calculation prints the consumption every month.

 
action_zoom_plus_stroke Meter trend log

Meter trend log

The calculation function supports negative meter consumption values, which can be used to handle cases where you need to subtract consumption, for example, when energy is produced on site.

When physically replacing an old meter with a new one, you have to configure the meter function of the trend log by adding the configuration and values of both the old and the new meter. These configurations and values are the foundation when handling a meter rollover or calculating consumption though meter replacement. For more information, see Managing Meter Replacement .

 
action_zoom_plus_stroke Manage replacement of meter dialog box where you enter the values of both the old and the new meter

Manage replacement of meter dialog box where you enter the values of both the old and the new meter

Note:
  • In order for a meter rollover to be managed correctly in the meter trend log and to ensure logging starts at the correct energy reading value, you enter previous meter and new meter information in the Manage replacement of meter dialog box. For more information, see Managing Meter Replacement .

  • Trend Log Types
  • Trends Overview
  • Trend Units
  • Log Record Storage
  • Managing Meter Replacement
  • Displaying Meter Change History
  • Create Trend Log Wizard – Initial Meter Settings Page
  • Change of Value Trend Log Properties – Meter Info Tab
  • Interval Trend Log Properties – Meter Info Tab
  • Manual Trend Log Properties – Meter Info Tab
  • Variable Triggered Trend Log Properties – Meter Info Tab
  • Extended Trend Log Properties – Meter Info Tab
  • Manage Replacement of Meter Dialog Box
  • Meter Change History Dialog Box