Use the Meter Info tab to configure the meter function of the trend log.
Meter Info tab
Property |
Description |
Is meter log |
Displays True if the trend log meter function is active. For more information, see Meter Function . |
Meter change time |
Displays the time when the meter was changed. |
Meter change user |
Displays the name of the user account that changed the meter. |
End time |
Displays the time when the old meter was replaced. |
End value |
Displays the value the old meter had when it was replaced. |
Start time |
Displays the time when the new meter was installed. |
Start value |
Displays the value of the new meter when it was installed. |
Meter constant |
Displays the constant of the new meter. If the meter counts in kilo (10 3 ), the constant is 1000. |
Min value |
Displays the first value of the new meter after roll-over. |
Max value |
Displays the last value of the new meter before roll-over. |