Product version: 1.7, 1.8, 1.9
6/25/2015

Trend Chart Settings Dialog Box – Calculation Tab

Use the Calculation tab to attach a calculation method to a series.

 
action_zoom_plus_stroke Calculation tab
Figure: Calculation tab

Table: Calculation Tab

Component

Description

Name

Displays all series in the trend chart. Select a series to display its presentation properties.

Calculation method

Select the calculation method to calculate the recorded values before displaying the series in the trend chart.

Delta over period

Select to apply a period to the delta calculation method.

Period

Select the time span for which the calculation method is to be executed.

Custom period

When Custom period is selected, enter a custom time span for which the calculation method is to be executed.

Custom period alignment

When Custom period is selected, enter the time when you want the custom period to start.

  • Trend Chart Series in WebStation
  • Trend Series
  • Trend Chart Series Menu
  • Trend Chart Settings Dialog Box – Axis Tab
  • Trend Chart Settings Dialog Box – Series Tab