earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: Trends
Product version: 1.7, 1.8, 1.9
6/25/2015

Trend Chart Settings Dialog Box – Axis Tab

Use the Axis tab in WebStation to change the settings for the x axis, y axis, and grid line of a trend chart.

 
action_zoom_plus_stroke Axis tab

Axis tab

Table: Axis Tab

Component

Description

Time mode

Select the time mode of the x axis.

Start time

Enter the absolute start time when Time mode is set to Absolute . This time is the leftmost point of the x axis. For more information, see Configuring the X Axis with an Absolute Time Span .

Time span

Type the relative time span of the x-axis when Time mode is set to Relative . The rightmost point of the x axis is the current time. For more information, see Configuring the X Axis with a Relative Time Span .

Show gridlines

Select True to show gridlines originating from the x axis scale. For more information, see Showing Trend Chart Grid Lines .

Auto scale left axis

Select True to activate auto scale. The scale of the left axis automatically adapts to the displayed series. For more information, see Automatically Configuring the Y Axis Scale .

Clear to deactivate auto scale. Manually scale the left axis by typing values in the  Minimum and Maximum boxes.

Minimum

Type the minimum value of the left axis. For more information, see Manually Configuring the Y Axis Scale .

Maximum

Type the maximum value of the left axis. For more information, see Manually Configuring the Y Axis Scale .

Show grid lines

Select True to show grid lines originating from the left axis scale. For more information, see Showing Trend Chart Grid Lines .

Auto scale right axis

Select True to activate auto scale. The scale of the right axis automatically adapts to the displayed series. For more information, see Automatically Configuring the Y Axis Scale .

Clear to deactivate auto scale. Manually scale the right axis by typing values in the  Minimum and Maximum boxes.

Minimum

Type the minimum value of the right axis. For more information, see Manually Configuring the Y Axis Scale .

Maximum

Type the maximum value of the right axis. For more information, see Manually Configuring the Y Axis Scale .

Show grid lines

Select True to show grid lines originating from the right axis scale. For more information, see Showing Trend Chart Grid Lines .

  • Trend Chart Axes in WebStation
  • Trend Series
  • Configuring the X Axis with an Absolute Time Span
  • Configuring the X Axis with a Relative Time Span
  • Showing Trend Chart Grid Lines
  • Automatically Configuring the Y Axis Scale
  • Manually Configuring the Y Axis Scale
  • Trend Chart Settings Dialog Box – Calculation Tab
  • Trend Chart Settings Dialog Box – Series Tab