earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Trends
Product version: 1.7, 1.8, 1.9
6/25/2015

Manually Configuring the Y Axis Scale

You manually configure the trend chart y axis to have a fixed scale. The trend chart has two y axes, one to the left and one to the right. You can use this procedure to scale both axes.

Show More
action_close

The x-axis of the trend chart represents time. The time span of the axis can be set with a fixed start and end time or with an end time relative to the present time. The axis can be quick-scaled to show the last hour, last day, last month, or last year​.

 
action_zoom_plus_stroke Absolute time span and relative time span, schematic

Absolute time span and relative time span, schematic

The y-axis refers to the measurement unit that the variable represents. The scale of the y-axis can be set manually or by auto scale. You can configure the trend chart to present series on one y-axis or two y-axes, one to the left and one to the right. Use two y-axes to present series with different ranges in the same trend chart.

 
action_zoom_plus_stroke One y-axis and two y-axes, schematic

One y-axis and two y-axes, schematic

To make reading easier, grid lines can be shown in the trend chart. Grid lines can be shown in both the x- and y-direction, independent of each other.

 
action_zoom_plus_stroke Grid lines, schematic

Grid lines, schematic

To manually configure the y axis scale
  1. In WebStation, in the System Tree pane, select the trend chart you want to configure.

  2. On the Trend Chart toolbar, click Settings .

  3. In the Auto scale left axis box and the Auto scale right axis box, select False .

     
    action_zoom_plus_stroke
  4. In the Left axis Minimum and Maximum boxes, type the minimum and maximum value of the left axis.

  5. In the Right axis Minimum and Maximum boxes, type the minimum and maximum value of the right axis.

  6. Click OK .

  • Trend Chart Axes in WebStation
  • Configuring the X Axis with a Relative Time Span
  • Configuring the X Axis with an Absolute Time Span
  • Showing Trend Chart Grid Lines
  • Automatically Configuring the Y Axis Scale
  • Saving Current Trend Chart Settings
  • Trend Chart View
  • Trend Chart Settings Dialog Box – Axis Tab