earth_america
user_standard Log on
action_search_stroke
earth_america

RP Controller Expansion Modules

RP-C-EXT-DALI-M-PD
RP-C-EXT-DALI
RP-C-EXT-0-10V-4-PD
RP-C-EXT-0-10V-4
RP-C-EXT-BL-SMI-4-HV-PD
RP-C-EXT-BL-SMI-2-LV-PD
RP-C-EXT-BL-4-HV-PD
RP-C-EXT-BL-2-LV-PD
RP-C-EXT-REL-4
CRS-HH-REL-10
RP-C-EXT-MS-BLE
RP-C-EXT-KNX
RP-C-RC-BLE
Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

128 Topic(s)

Concept

The RP controller Modbus RTU (RS-485) subnetwork allows standard Modbus devices and the KNX Modbus gateway (RP-C-EXT-KNX) to be connected to the controller.

How to

You connect RP controller expansion modules and multi-sensors to the RP-C room bus to provide the devices with power and communication from the RP-C controller.

Concept

The RP controller room bus allows RP controller expansion modules to be connected to the controller for people counting, motion detection, luminosity and sound pressure level measurements, Bluetooth Low Energy based applications, and control of electric lights and window blinds.

Concept

The wiring recommendations for the communication ports on the automation servers, BACnet/IP devices, RP controller expansion modules, and Operator Display devices apply to wires and cables used for RS-485 communications, LonWorks communications, USB connections, Ethernet connections, sensor bus connections, room bus connections, and RP controller Modbus network connections. Always use the recommended cables and wires.

Specifications

Concept

The RP controller expansion multi-sensor can be installed on a dropped (suspended) ceiling, a drywall ceiling, or a junction (gang) box.

Concept

The Schneider Electric SpaceLogic hardware devices for the EcoStruxure BMS include terminal bases, PS-24V power supplies, Central IO modules, automation servers such as AS-P servers and AS-B servers, BACnet/IP devices such as MP-C controllers, MP-V controllers, IP-IO modules, and RP-C controllers, RP controller expansion modules, remote control, KNX Modbus gateway, Bluetooth adapter, Wireless Adapter - Advanced, SpaceLogic Sensor devices, Advanced Display devices, and Operator Display devices.

Concept

The RP-C-EXT-MS-BLE multi-sensor connects to the RP-C room controllers and is used for infrared motion detection and luminosity measurements. The multi-sensor supports Bluetooth Low Energy based applications such as beaconing and remote control communication. ​

Concept

This section provides information on regulatory compliance and approvals for the RP controller expansion sensor modules of the Multi-sensor model.

Concept

RP controller expansion modules have two types of memory, flash memory and RAM.