earth_america
user_standard Log on
action_search_stroke
earth_america

WorkStation

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

405 Topic(s)

Specifications

Concept

You use trend logs to record values, such as a sensor. A trend log can also log consumptions, such as energy consumption or water consumption.

Concept

You can add attachments to alarm objects, except System Information alarms. An attachment is a link pointing to an object in the system. When an alarm that has an attachment is triggered, a paperclip icon is displayed in the Alarms pane and Alarm Views. It is also possible to configure the attachment to display when the alarm is going from Normal to Alarm state.

User Interface

Use the User menu to access useful shortcuts from various menus in Workstation.

Concept

Content types are predefined layouts that you save to reuse for specific types of folders or container objects.

Concept

Concept

There are a number of different clients, servers, and features that requires licenses to operate.

How to

You duplicate an EcoStruxure BMS server from a backup set using Restore when you want to reuse configuration data from a backup set in a standalone automation server.

User Interface

Use the Rename object dialog box to rename an object.

Concept

You can use the Restore function to re-use the configuration data from a backup set in a new standalone automation server. Rather than manually configuring your preferred automation server configuration, you can save time and configure the standalone automation server from a backup set.