939 Topic(s)
You can use a service_blacklist to direct the EcoStruxure BMS server to send ReadProperty requests, rather than ReadPropertyMultiple requests. They are used to request multiple attributes of different objects with a single request.
Values in Building Operation are stored in the Building Operation database with all input decimals. If a stored value consists of more decimals than the operating system is defined to display, the value is rounded off according to the operating system settings before it is displayed in WorkStation.
You configure an alarm decoration rule to change the properties that are overridden.
You configure the properties of an enumeration alarm to meet the unique needs of your site.
You configure the properties of a sum alarm to meet the unique needs of your site.
You configure the properties of a out of reference range alarm to meet the unique needs of your site.
You configure the properties of an out of range alarm to meet the unique needs of your site.
You configure the properties of a change of state alarm to meet the unique needs of your site.
You configure the properties of a matching text string alarm to meet the unique needs of your site.
You configure the properties of a multistate alarm to meet the unique needs of your site.