11 Topic(s)
This section provides information on regulatory compliance and approvals for Wireless Adapter - Advanced.
You install Wireless Adapter - Advancedr on a wall using the mounting cradle and wall plate and connect the adapter to an RP-C controller, AS-P server, or AS-B server to add Zigbee wireless connectivity to the controller or server.
You install Wireless Adapter - Advanced in a dropped ceiling and connect the adapter to an RP-C controller, AS-P server, or AS-B server to add Zigbee wireless connectivity to the controller or server.
You install Wireless Adapter - Advanced on the exterior of a metal enclosure and connect the adapter to an RP-C controller, AS-P server, or AS-B server to add Zigbee wireless connectivity to the controller or server.
Wireless Adapter - Advanced is a USB-based wireless adapter that enables ZigbeeTM wireless connectivity with an RP controller, AS-P server, or AS-B server, extending the controller's or server's point count and bringing flexibility in retrofit applications.
The Schneider Electric SpaceLogic hardware devices for the EcoStruxure BMS include terminal bases, PS-24V power supplies, Central IO modules, automation servers such as AS-P servers and AS-B servers, BACnet/IP devices such as MP-C controllers, MP-V controllers, IP-IO modules, and RP-C controllers, RP controller expansion modules, remote control, KNX Modbus gateway, Bluetooth adapter, Wireless Adapter - Advanced, SpaceLogic Sensor devices, Advanced Display devices, and Operator Display devices.
This section provides information on the wireless devices that are supported by the wireless network.
The EcoStruxure Building Operation software supports the major communication protocols in building automation and security management.