earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Registration Portal
Functionalities: Registration
Product version: 1.5, 1.6, 1.7, 1.8, 1.9
5/23/2018

Viewing Updated Registration Information in WorkStation

You can view the registration information in WorkStation that was updated in SmartStruxure Registration Portal.

Show More
action_close

You register a Building Operation system online when WorkStation is connected to the Internet. When you log on to WorkStation, you are prompted to register your system. You can register immediately or at a later time.

You can register at any time in WorkStation by clicking Help > Registration .

To confirm the system registration, the end-user must provide consent for sharing system information and personal information.

For more information, see Providing Your Consent on Sharing System Information .

For more information, see Providing Your Consent on Sharing Personal Information  .

Important:

Each stand-alone SmartStruxure server device is considered as a new registration. If a stand-alone SmartStruxure server device is then attached to the Enterprise Server, the SmartStruxure server device’s registration information is overwritten by the Enterprise Server’s registration information.

If the stand-alone SmartStruxure server devices are to be attached to the Enterprise Server later, it is recommended not to register the SmartStruxure server devices.

Note:

Ensure that WorkStation is connected to the internet.

To view updated registration information on WorkStation
  1. In WorkStation, on the Help menu, click R egistration .

  2. Click Edit information .

     
    action_zoom_plus_stroke
  3. Log on to SmartStruxure Registration Portal.

  4. Click Edit .

     
    action_zoom_plus_stroke

  5. Click Submit .

     
    action_zoom_plus_stroke

  6. In WorkStation, on the Help menu, click Registration .

     
    action_zoom_plus_stroke
  • Online Registration
  • Offline Registration
  • Registration Information Dialog Box for Online System
  • Registration Information Window for Offline System Registration
  • Systems – Installation Tab
  • Edit Systems – Installation Tab
  • Editing System Installation Information