Custom View lists the objects and functions that are available in the Custom View folder of Building Operation in a logical manner, such as hierarchical, geographical, or functional. So, you do not see the entire tree structure of WorkStation, just the parts that you want to see or all the parts in the order that you want. For example, in WorkStation, you create a Custom View that contains variables of a Campus that you want to monitor from Technician Tool.
To have Custom View on Technician Tool, an engineer needs to create the Custom View folder in WorkStation consisting of the functions and objects in the order that you want. You can then view and navigate through the system objects using Custom View on Technician Tool.
For more information, see Creating Custom View Folder in WorkStation
.
The values of the grayed out variables without the
Force
option are read-only values that you can not change.
The values of the grayed out variables with the
Force
option can be changed when you force
ON
.
For more information, see Forcing a Value
.
A warning icon next to a variable means that the value cannot be converted and may not represent what you are expecting to see. For example, the power consumption variable cannot have units in g/m
2
. The unit should be kWh. This error is represented by warning icon.
The value is displayed in blue font when the value is not older than 3 minutes and there is no network failure.
Using the built-in swipe-to-refresh feature, values and objects can be easily refreshed in
Custom View
as well as within a particular folder in
Custom View
.
You can scroll through the long list of objects and variables in
Custom View
as well as within a particular folder in
Custom View
using quick scroll bar.
Objects and variables are listed in the same order as in WorkStation.
Note:
Objects and variables listed in
Custom View
vary according to the software permissions assigned to the user who has logged into Technician Tool.
For more information, see User Account Profile Workflow
.
action_zoom_plus_stroke
Custom View in iOS and Android
Trend Logs
You can view a list of trend logs and their properties. You can filter the trend logs based on date and time as well as search logs based on value. You can view the name, type, and source of trend log.
For more information, see Viewing Trend Logs
.
action_zoom_plus_stroke
TrendLogs for iOS and Android
Schedules
You can view a list of schedules and manage a schedule. Schedule operations are the same as in WebStation.
Schedules are used to schedule the operation of part of the building management system, such as a fan, a door, or a setpoint. Using a schedule, a fan can be set to operate between 08:00 and 17:00 every workday.
Schedules can be overridden by different types of exceptions. For example, if you want to shut the fan down the last Friday in every month due to maintenance, you can use a calculated exception. The exception is added to the schedule and turns off the fan the last Friday in every month.
If you want to shut down the fan during the summer vacation, you can use a Calendar exception. In this case, you use an already created calendar that defines the summer vacation. This calendar is added to the schedule as an exception and the fan will be shut down during all days of the summer vacation defined by the calendar.
You can view schedule details only in landscape mode.
For more information, see Viewing Schedules
.
action_zoom_plus_stroke
Schedules for iOS and Android
Graphics
You use graphics to display building overviews, display values from sensors, or change setpoints. A graphic can also contain links to trend charts, trend log lists, Internet sites, or views in WorkStation and WebStation.
You can view graphics only in landscape mode and also refresh the graphics.
Note:
Panel objects are not supported in Graphics.
action_zoom_plus_stroke
Graphics in iOS
action_zoom_plus_stroke
Graphics in Android