earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server
Functionalities: Hardware
Product version: 1.7, 1.8, 1.9, 2.0, 2.1, 3.0, 3.1
8/20/2020

Automation Server Communication Ports

The Automation Server has the following communication ports:

  • 1 Ethernet 10/100 megabit port

  • 2 RS-485 ports

  • 2 LonWorks (TP/FT and RS-485) ports

  • 2 USB host ports

  • 1 USB device port

  • 1 backplane I/O bus port

Table: Automation Server Communication Ports

Communication port

Connection

Ethernet 10/100

IP, LAN/WAN, Modbus, BACnet

RS-485 COM A

Modbus, BACnet

RS-485 COM B

Modbus, BACnet

LonWorks (FT and RS-485)

LonWorks

USB host

USB device

Device Administrator

Backplane I/O bus

Internal power supply and I/O addressing

There are two USB host ports facing down to connect to external devices, such as ADs. The USB device port on the front is intended for program download from a PC by means of Device Administrator. It is connected to a PC or a downstream port of a hub.

The Ethernet communication is performed over a 10/100BaseTX, 10 or 100 Mbps, twisted pair network. The network is connected to the Automation Server by an RJ45 connector.

  • Hardware Overview
  • Automation Servers
  • AD v1
  • AD v2