earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Alarms
Product version: 1.9
12/14/2016

Multistate Alarm Properties – Alarm Settings Tab

Use the ​ Alarm Settings tab to change the alarm properties of a multistate alarm.

 
action_zoom_plus_stroke Alarm Settings tab

Alarm Settings tab

Table: Alarm Settings Tab

Property

Description

Acknowledgement type

​Select the type of acknowledgement for the alarm.

For more information, see Acknowledgements .

Alarm message

Type the message to display when the alarm is in Alarm state.

For more information, see Alarm Messages .

Reset message

​Type the message to display when the alarm is reset.

Alarm priority

Enter the priority level of the alarm.

For more information, see Priority .

Reset priority

​Enter the priority level of the alarm when it is reset.

For more information, see Priority .

Category

​Enter the category that the alarm belongs to.

For more information, see Categories .

Cause note group

​Enter the cause note group that is used by the alarm.

For more information, see Cause Notes .

Action note group

​Enter the action note group that is used by the alarm.

For more information, see Action Notes .

Checklist

​Enter the checklist that belongs to the alarm.

For more information, see Checklists .

Checklist required

Select to require that a checklist is filled in before acknowledging an alarm.

Prefix for alarm source name

Type a prefix that is added to the beginning of the source name property of an alarm record.

Disable alarm

Select to disable the alarm, for example, before deployment.

For more information, see Disable and Enable Alarms .

Auto hide

Select to automatically hide the alarm in the Alarms pane or Alarm View.

For more information, see Hide and Show Alarms .

Disable state-change logging

Select to prevent an alarm state change from creating an event.

For more information, see Alarm State-Change Logging .

F lashing alert

Select to make the alarm row flash in the Alarms pane and Alarm Views when the alarm is triggered.

Audible alert

Select to make the alert audible when the alarm is triggered.

 
action_zoom_plus_stroke
(Action Requirements)

Edit

Click to open the property pane where you edit the selected user action. For more information, see User Action Properties .

 
action_zoom_plus_stroke
(Attachments)

Add

Click to open the Create Object: Attachment wizard, where you add an attachment. For more information, see Create Object Wizard – Naming the Object Page .

 
action_zoom_plus_stroke
(Attachments)

Edit

Click to open the property pane where you configure the attachment. For more information, see Attachment Properties .

 
action_zoom_plus_stroke
(Attachments)

Remove

Click to remove an attachment that is connected to the alarm.

  • Multistate Alarms
  • Multistate Alarm Properties – Basic Tab
  • References Tab
  • Acknowledgements
  • Alarm Messages
  • Priority
  • Categories
  • Cause Notes
  • Action Notes
  • Checklists
  • Disable and Enable Alarms
  • Hide and Show Alarms
  • Alarm State-Change Logging
  • User Action Properties
  • Create Object Wizard – Naming the Object Page
  • Attachment Properties
  • Alarm Substitution Codes