earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 1.9
10/12/2017

System Alarm ID NW8 S-NW8 Z

Listed below are the System Alarms with IDs that begin with the letters NW8 S-NW8 Z.

Table: System Alarms NW8 S

System Alarm ID

Description

NW8 Sensor input failure

The controller has detected an input sensor range failure.

NW8 Setpoint out of range

The Flo2 Remote Setpoint is enabled and out of range.

NW8 System fault 32

Missing changeover input for an MnHpfc fan coil application.

Table: System Alarms NW8 U

System Alarm ID

Description

NW8 UI diagnostic

The measured input value at UI:xx (from UI:1 to UI:8) is outside the standard range for the configured sensor for a MICROZONE II controller.

NW8 Unrecognized command

The controller did not recognize the command.

Table: System Alarms NW8 Z

System Alarm ID

Description

NW8 Zone temperature out of range

The MicroFol II zone temperature is out of range.

  • System Alarm ID List
  • System Alarms
  • System Alarm ID A-D
  • System Alarm ID E-L
  • System Alarm ID M-NW8 R
  • System Alarm ID P-S
  • System Alarm ID T-X