earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Alarms
Product version: 1.9
12/14/2016

Write to File Notification Distribution Method

The write to file notification is written to a text file when the configured notification condition is met.

You can use the write to file notification distribution method, for example, to trigger a third-party software program that sends an SMS to a recipient when a specific text string is written to the file by a SmartStruxure server. For more information, see Create Notification Wizard - Configure Write to File Page .

You can configure whether new information is appended to the existing file, overwrites the current content of the file, or if it is written to a unique file. By default, new information is appended to the existing file. If the file does not exist, a new text file is created.

The text file is saved in the Building Operation database folder: '...db/notifications'. You can access the notification file from the WorkStation 'System' folder, 'Notification files' subfolder of the SmartStruxure server where the file was generated. You can open the notification file with a text editor installed on the computer.

You can save the file to a different location and rename it. You can also delete the notification file.

Important:

When you delete the notification file, it is deleted from the physical device.

  • Notification Distribution Methods
  • Create Notification Wizard - Configure Write to File Page
  • Accessing a Notification Written to a File
  • Saving a Notification Written to a File
  • Deleting a Notification Written to a File
  • Email Notification Distribution Method
  • SNMP Notification Distribution Method