Use the Alarm Triggered Notification view to view and edit the configuration of an alarm triggered notification.
Alarm triggered notification view
Number |
Description |
![]() |
Properties Use the properties to configure how the notification is activated, what notification report to connect to the notification, and what properties to use for the notification text. For more information, see Alarm Triggered Notification Properties - Basic Tab .. |
![]() |
Notification text Use the notification text to edit the contents and formatting of the notification text. For more information, see Notifications .. |
![]() |
Quick filter Use the Quick filter to enter a word to filter on. For more information, see Quick Filter .. |
![]() |
Substitution codes list Use the alarm substitution codes list to select the data you want to include in the notification. For more information, see Alarms Substitution Codes .. |
![]() |
Distribution method Use the distribution method to start a wizard where you configure how the notification is distributed. For more information, see Create Object Wizard - Configure Email Page . For more information, see Create Notification Wizard - Configure SNMP Page . For more information, see Create Object Wizard - Configure Write to File Page . |
![]() |
Filter Settings Use the filter settings to select the alarm filter conditions that have to be met before the notification is triggered. For more information, see Alarm Filters .. |