earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, IP-IO , MP-C
Functionalities: Hardware
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022
7/22/2021

Keys

You use the keys on the override display to navigate the screens of the user interface and to select options on menus and lists.

Table: Keys

Key

Description

 
action_zoom_plus_stroke

Home  

Press to go to the Home screen.

Press and hold down for three seconds to enter the configuration mode and go to the I/O Configuration screen. For more information, see I/O Configuration Screen .

 
action_zoom_plus_stroke

Back  

Press to return to the previous screen.

 
action_zoom_plus_stroke

Up/previous  

Press to scroll in a menu or list and to highlight an option.

Press to increase a value.

 
action_zoom_plus_stroke

Down/next  

Press to scroll in a menu or list and to highlight an option.

Press to decrease a value.

 
action_zoom_plus_stroke

Enter

Press to go to from the Home screen to the I/O Filter screen. For more information, see I/O Filter Screen .

Press to select an option in a menu or list and go to the next screen.

Tip:

Press and hold down the Up/previous key

 
action_zoom_plus_stroke
or Down/next key
 
action_zoom_plus_stroke
to speed up scrolling in the override display menus and lists.

  • AS-B Servers
  • MP-C Controllers
  • Output Override Function
  • I/O Configuration Screen
  • I/O Filter Screen