You can customize the presentation of decimals, value types, width, and alignment in a notification text or a notification report text.
You can customize the presentation of the number of decimals using the following text formatting codes:
Code |
Description |
@(Value) |
Displays 2 decimals |
@(Value:%.1f) |
Displays 1 decimal |
@(Value:%.4f) |
Displays 4 decimals |
The default number of decimals displayed in a notification or notification report is two.
You can customize the presentation of the value types using the following text formatting codes:
Code |
Description |
t |
Value type |
s |
String |
f |
Float |
You can customize the width and alignment of data in a notification or notification report using the following text formatting codes:
Code |
Description |
%wt |
At least w wide, right aligned |
%-wt |
At least w wide, left aligned |
%=wt |
At least w wide, center aligned |
%w.ct |
At least w wide, right aligned, max c long |
%-w.ct |
At least w wide, left aligned, max c long |
%=w.ct |
At least w wide, center aligned, max c long |
In this example, we have an alarm with the source '/Server/Alarm1' with a monitored value of 0.5.
This alarm has the source '/Server/Alarm1'