earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Engineering, User Management
Product version: 1.9
10/12/2017

Customized Navigation Workflow

Use this workflow to create a customized navigation pane in a workspace or panel.

 
action_zoom_plus_stroke Create a customized navigation pane flow chart

Create a customized navigation pane flow chart

Create a menu

Create a menu object to be used in the navigation pane.

For more information, see Creating a Menu .

Create a workspace or a panel

Create the workspace or panel where you want to add the navigation pane.

For more information, see Creating a Workspace .

For more information, see Creating a Panel .

Add a navigation pane to the workspace or panel with the menu as initial path

Add a navigation pane to the workspace or panel and use the menu as initial path.

For more information, see Adding a Component to a Workspace .

For more information, see Creating a Panel .

  • Customized Navigation
  • Creating a Menu
  • Creating a Workspace
  • Creating a Panel
  • Adding a Component to a Workspace