Functionalities: Trends
Product version: 3.2, 3.3, 2022
10/15/2020

Disabling a Trend Log

You disable a trend log to stop recording values.

Show More
action_close

​The interval trend log and change of value trend log start recording values when the configured activation conditions are met. If an activation variable is used, both the activation variable and the activation time have to be true for the trend log to start recording.

On all trend logs, you can stop recording values by disabling the trend log. To resume recording, you enable the trend log. For more information, see Disabling a Trend Log .

Activation Variable

You configure an activation variable to have the trend log start recording values when a connected variable goes on. This variable can be a scheduled variable or a variable from a switch.

You can also have the trend log stop recording when the variable, such as a fan, goes off. For example, you can use this feature to log the effective time a fan is on.

 
action_zoom_plus_stroke Activation variable that follows the activation time

Activation variable that follows the activation time

Start at activation time

You configure an activation time to have the trend log start recording values at a specified time.

For Interval Trend Logs, the logging interval is aligned with the activation time. For more information, see Interval Trend Logs .

 
action_zoom_plus_stroke Trend log that starts recording at activation time

Trend log that starts recording at activation time

To disable a trend log
  1. In WorkStation, in the System Tree pane, select the folder or EcoStruxure BMS server where the trend log is located.

  2. Select the trend log you want to disable

  3. On the Actions menu, point to Activation and then click Disable trend log .

The trend log is now disabled.

  • Enabling a Trend Log
  • Trend Log Activation
  • Actions Menu – Activation Submenu