earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WorkStation, WebStation
Functionalities: Basic Functionality
Product version: 1.1, 1.2, 1.3, 1.4, 1.5, 1.6, 1.7, 1.8, 1.9
6/23/2011

Hiding Panes

You hide panes if you do not use them or think they take up too much space.

Show More
action_close

The workspace in WorkStation and WebStation is the area where you perform all tasks at your site, such as acknowledging alarms and viewing trend logs.

The workspace is made up of different components, such as panes, lists, and views. These components can be configured in a number of different ways. You can hide or display components and create and save your own workspace. You can also reset the workspace layout to the default layout for the user group your user account belongs to.

WebStation uses cookies to remember your workspace when you log off. When you log on again, you get the workspace you used when you logged off. If you clear your web browser, you will regain the default workspace.

 
action_zoom_plus_stroke Workspace in WorkStation (left) and WebStation (right)

Workspace in WorkStation (left) and WebStation (right)

Some objects have specific views in WorkStation and WebStation:

  • Alarms

  • Documents

  • Graphics (TGML)

  • Events

  • Trend Charts

  • Trend Log Lists

  • Schedules

  • Calendars

  • Watch

When you open an object that does not have a specific view, the Properties dialog box for that object is displayed.

Panels

Panels are a way to create workspaces that display two or more components in Building Operation, for example graphics, trend charts, trend list and alarm views.

For more information, see Panels .

Web Pages

Web pages on the Internet can be displayed in the Workspace in Building Operation.

For more information, see Web Pages .

To hide panes
  • In WorkStation or WebStation, click View and then click the panes you want to hide.

  • Customization
  • Workspaces
  • View Menu
  • View Menu
  • Increase the Work Area in WorkStation
  • Hiding Menus and Toolbars